因为电路上有用到SN6501隔离+5V转±5V的电源应用,
但还需要一组+5V转±15V的电源,所以打算用SN6501来做设计,
±15V的应用不需要隔离,最大负载电流±50mA,
请问此应用可以实现吗?
参照数据表 Figure 48来设计新的变压器吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
参照datasheet 22页图46/48是可以设计输出+/-15V, 但是这个芯片做达到最大负载50mA., 你可以考虑用SN6505来做。*变压器重新设计)
同时你不需要隔离,或可以采用TPS61093/TPS61080来做, 例如参照TPS61093 datasheet第16页figure16, 不需要用到变压器,主要注意功率电感饱和电流足够,修改反馈输出15V即可,-15V是对称输出。。
Hi Johnsin
感谢回复
再请问,如果可以建议用电荷泵来产生负电源,
其他TI相关的升压IC应该也是可以参照应用?
不一定得采用TPS61093/TPS61080来做?