This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于 扫地机充电设置



各位大神们? 3串三元电池组,扫地机 充电模式设置为: 12.4V之前是恒流CC600mA充电,当检测到电压达到为12.4V时候,改为cv涓流充电 12.6V时长设置为40min。电芯容量为2500mAH.这样设置合理吗?  个人觉得 12.6V设置电压会有个 0.15V误差 ,电池组 可能 会充电到12.75V单节电芯可能会充到4.25V以上,长期如此会造成电芯损坏。   各位大神们有什么建议,看法?