If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
200mA以内可以用chargepump,直接正压转负压,无电感,电路简单,但是因为有输出阻抗,5V输入,依据电流,输出会偏离-5V一些,例如-4.8V.
如果电流大,例如超过200mA, 可以用降压转换器来做,例如TPS62150, 参照:
Using the TPS6215x in an Inverting Buck-Boost Topology (在TPS62150官网应用手册中找,这个设计支持500mA左右输出,如果要更大电流可选择这个芯片高电流版本,例如TPS62130A)