This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ20Z60-R1中的ICC位



问题描述:Pump在充电时报警,(经分析是因为Pump里的一块控制板抓取不到电池电量信息),重新启动一次后,所有现象全部消失,多次测试都没有复现问题。

 

经过分析比较IC的说明书后有下列疑问:

  1. ICC位的不同表示的具体含义?为什么状态有的为“1”,有的为“0”?

  2. ICC是控制电池的那块功能的? (是否与信号传送有关系)

  3. ICC置位的状态是否与信号传送有关系?

  4. 规格书上说明ICC 是只读位,当ICC位初始为1时,为何我们可以修改该ICC位为0后读出数据为0?