Other Parts Discussed in Thread: LM27761, ADC08D500, TPS65251
给公司设计了一个高速数据采集卡,正常使用12V供电,电源入口芯片使用TPS65251,设计及输出电流电对应1.2V-3A、2.5V-2A、3.3V-2A。1.2V对应负载为Spartan6 LX100、CYUSB3014内核供电。2.5V对应负载为LDO转1.9V供ADC08D500、及FPGA IO。3.3V负载对应FPGA IO、AD9517-3 PLL、LDO转1.8V供FPGA IO用、使用LM27761及LP38698SD转出±2.5V供两个运放使用。
从电源入口测试进行数据采集传输时电流为0.31A,对应功耗3.72W,单独测量各路功耗均不大,由于设备在现场大部分时间处于常温状态,目前现场的数据采集卡未出现过问题,但是正常出厂测试都需要高低温(-10到55度),高温未出现过问题,问题集中出现在低温环节,低温-10度TPS65251可能会出现某一路输出损坏,目前3.3V输出损坏较多,1.2V出现过损坏后输出电压偏高,实际测试3.3V对应输出电流0.5A左右。室温工作芯片温度只比室温高一点,摸上去只能感受到一点点发热,由于目前故障主要出现在该芯片,因此希望大家看看我的电路是否存在问题,电路参考TPS65251 High Current, Synchronous Step Down Three Buck Switcher Evaluation Module设计,电感使用的同一型号