This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3409 FET驱动疑问,出现烧MOS问题



文档的17页有一个关于FET电路的图 Figure 27. External Parallel FET Dimming Circuit。我目前电路是输入58V,输出54V 4A,我参考Figure 27的电路图。采用以下参数Coff是470P, Roff1:69.8k,Roff2:4.3K,VDD:12V.2个二极管用SS510。 一上电,电源直接保护,断电逐个检测,发现P管、N管烧了。后来去掉FET电路,换上新P管和电流 采样电阻。系统恢复工作。请问是我的二极管用错还是怎样?为什么会导致烧管子的?