This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB320 设计



客户需要实现支持12V输入,支持USB3.0(实际应用可能是通过HUB线实现DCIN+USB3.0).  对于这种应用,客户想确认下面的设计是否正确。只是用CC Controller 是否能够实现这种功能。第二用于配置控制的CC Controller 资料放在哪里?参考线路有通过SMBUS来控制的,是否需要额外添加一个ROM。