This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【FAQ】BQ76930:针对17S应用,推荐的电池配置是什么?



BQ76930     BQ76930 Datasheet

Q: 两个BQ76930器件有17个串联电池。针对17S应用,建议使用哪些电池配置?

L=低侧,H =高侧

配置1:10S(L)+7S(H).

配置2:9S(L)+8S(H).

配置3:8S(L)+9S(H).

配置4:7S(L)+10S(H).

A:bq76930的两个重要工作条件是:

1)在短路/重载条件下将VC5X保持在VSHUT以上;

2)为FET驱动器保持足够的REGSRC电压。

我会推荐配置2,因为如果使用的是TIDA-01093之类的电路的话,想让器件之间的电压大致相等则应该为每个器件提供良好的工作电压,并且由于下部器件的顶组中的电池数较少会降低短路时在VC5X上的负载。您的特定电路可能需要特殊考量,请根据需要使用模拟来协助分析,并确保测试您的解决方案。