This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bqStudio chemistry data flash for bq35100

Other Parts Discussed in Thread: BQSTUDIO, BQ35100, GPCCHEM

bqStudio  ver:1.3.86

bqStudio`s Chemistry function, I found my battery`s chem id, and Program selected chemistry OK.

battery info:EVE EVE_ER34615 (19000mAh)

why Program selected chemistry OK, but the data flash reg not be wiritten.

Gas Gauging :Cell Design Capacity mAh and so on, such these regs.

why? Gas Gauging`s regs config need myself program? not by Chemistry Programming?

thank you!

使用Chemistry 功能,找到了对应的电池 chem id

EVE EVE_ER34615 (19000mAh)

选择之后,然后Program selected chemistry,都是OK。Successfully programmed chemistry.

为什么Data Memory的 Gas Gauging :Cell Design Capacity mAh这些config的值都没有变化呢?

chem id读出的值到是变化了,是OK的。

是没有写入data flash吗?Gas Gauging 的配置需要自己配置?Chemistry Programming没有这个功能?

谢谢!