This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

急急急!bq25504的使用问题



我使用了该芯片,OV = 3.15V, UV = 2.2V, 我用直流电源作为输入VIN来模拟太阳能电池,VBAT接了一个超级电容(1F, 5.5v)作为储能器件,VSTOR接了个220欧姆的电阻,当我打开直流电源时,VSTOR两端有电压,VBAT在充电。当超级电容充电至3v时,我把直流电源关掉来模仿太阳能板在晚上的情况,此时VSTOR两端的电压直接变为0 ,按理说此时不是应该超级电容给vstor供电的吗? 这个问题困扰了我好久,我哪里操作错了吗?请知道原因的来回答一下吧,谢谢啦!文件里是我使用的电路图4718.CJMCU-25504.pdf