This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq40z50化学ID

Other Parts Discussed in Thread: BQ40Z50

TI工程师你好:

请问BQ40Z50 chemistry ID 使用Studio开始记录数据部分需要包含充电部分吗?还是充满后开始记录(包括静放那2小时),还是从放电才开始记录?

我之前提交过一次,TI发邮件给我说数据不对

谢谢

  • The required test consists of the following steps:
    1. Test is performed at room temperature. If the cell was at a different temperature , let the cell relax for
    two hours at room temperature prior to the test.
    2. Charge using CC or CV charging to full using taper current. (For example, C/100.) Use nominal CC
    charge rate and CV voltage. If another charging method is specified by the cell maker, use that
    method.
    3. Let the battery relax for two hours to reach full equilibrium open circuit voltage (OCV).
    4. Discharge the battery at C/10 rate until the minimal voltage (as specified by the cell manufacturer) is
    reached.
    5. Let the battery relax for five hours to reach full equilibrium OCV.
  • 这个5步的数据都需要记录下来吗?