大家好,最近使用TPS75005给28235进行供电时,两通道电压设置为1.9v和3.3v,进行多次重复上电(间隔时间为1s),测试偶尔出现3.3v输出异常(2.2v左右),1.9v电压始终正常,EN引脚电压使用电阻分压(始终为1.8v),不知道应该怎么解决。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,最近使用TPS75005给28235进行供电时,两通道电压设置为1.9v和3.3v,进行多次重复上电(间隔时间为1s),测试偶尔出现3.3v输出异常(2.2v左右),1.9v电压始终正常,EN引脚电压使用电阻分压(始终为1.8v),不知道应该怎么解决。
谢谢回复,核实了下原理图,3.3v只给28235的电源引脚进行供电,整个3.3v链路上电容不超过100uf。
您好
经过多次验证后,发现给tps75005供电的5v电源在下电后长时间保持在300mv(2s之内都是),再次上电后tps75005的1.9正常,3.3v上升到2.4v后出现跌落,跌落到2v左右。
将供电电源5v并联500Ω电阻到gnd后,再也没出现过3.3v异常的现象。
tps75005芯片介绍芯片下电是以两个通道都低于0.3v为标准,但是现在是输入端的5v没降到0.3v以下,1.9和3.3都已经降到了0.3以下。
现在排查的重点方向应该放在哪里呢。