This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

电源芯片中最大结温计算疑惑



我想请教下,结温的计算方法,一般公式都是写Tj=TA+(PD*θJA)

1.TA代表环境温度,是否是指室内环境温度,我是否可以假定为30℃?

2.PD为器件的功耗,PD公式是否为PD=|(Vout-Vin)| * Iout ? 那如果我是正5V转负5V,压差怎么计算?

3.最大的一个问题,我看一个芯片手册中封装处Tjmax=125℃,θJA=256℃/W,然而典型应用写着输入5V,输出12V/300mA,但是我按公式这样计算TJ=30℃+(12-5)V*0.3A*256℃/W=567.6℃远大于最大结温125℃????

我计算哪里有问题,崩溃中