This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FR9886 DC芯片



遇到的问题:共两块电路板,A板  24V转成12V供输入,输出为5V,但实际电压在四点几伏浮动,5v再通过LM1117-3.3V芯片后被拉低为2.9V;     

                        后参考手册,用B板  将R2 R3分别改为44.2K和10K,L3改为10UH功率电感。测得输出电压拉高为8.7V,用万用表量两块的FR9886的FB脚,电压都不是参考的0.925V。麻烦大神帮忙解解惑