This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Load select 的8种负载类型怎么选择?



0~7共8种负载选择,它们都应用在什么场景的?有想关的资料吗?

  • 图片不显示? 如下规格书中的8种,应用场景是不同的吗?

    0 = Average discharge current from previous cycle: There is an internal register that records the
    average discharge current through each entire discharge cycle. The previous average is stored in
    this register.
    1 = Present average discharge current: This is the average discharge current from the beginning of
    this discharge cycle till present time.
    2 = Current: based off of Current
    3 = Average Current (default): based off the Average Current
    4 = Design Capacity / 5: C Rate based off of Design Capacity /5 or a C / 5 rate in mA.
    5 = AtRate (mA): Use whatever current is in AtRate
    6 = User_Rate-mA: Use the value in User_Rate-mA. This gives a completely user configurable
    method.
    7 = Maximum of Average Current from the previous discharge cycle.
  • 这个文档在哪里看到的,请发一下链接。
    0-7看起来有点像参数定义
  • SLUA511B 第65页,load select
  • 建议您选default值,选择不同的电流模式计算剩余容量