使用BQ24707制作的充电板,在上电后,充电参数配置正确,但是过几秒后DHIDRV侧的MOS烧毁。 下面是充电的参数,以及测试的电压:
设计参数为:8.6-24V输入;4A充电;8.6V的充电电压。
主要的电压测量如下:
输入电压 :11.86V
ILIM电压 : 0.8V
ACDET电压:3.19V
REGN 电压: 6V
BTST电压: 10.75V
请问可能是什么原因。附件中是原理图,与BQ24707的示例基本相同。 1602.ChargeByIC.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用BQ24707制作的充电板,在上电后,充电参数配置正确,但是过几秒后DHIDRV侧的MOS烧毁。 下面是充电的参数,以及测试的电压:
设计参数为:8.6-24V输入;4A充电;8.6V的充电电压。