- 能否恒定的达到最大2.1A持续供电? 我们后端实际功率可能在8~9W左右,但峰值可能到12W,感觉有点不够。
- 这颗料也支持路径管理在适配器插拔的时候,boost输出的5V是怎么样变化的? 从boost转为buck给锂电池充电?
- 能否不使用boost功能,只输出电池或buck供电? 因为我们后端设计支持范围很宽3.0~5.2V都可以。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.