This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

急急急,关于BQ24195加无线充电方案拖死问题

Other Parts Discussed in Thread: BQ24195

工程师你好!

我们公司一款平板搭配NE6101无线接收IC给BQ24195充电遇到如下问题,请帮忙分析下:

无线接收IC的功率有10W(9V,1.1A)或者5W(5V,1.1A),但总会被BQ24195拖死

1.正常情况下,输入电流限制1.2A,充电电流限制为1.6A,但实际测量充电时瞬间输入电流高达1.7A左右,且无线接收IC因功率过载而与TX端断开连接

2.输入电流限制0.5A,充电电流限制为0.5A,但实际测量充电时瞬间输入电流高达1.5A左右,且输入电流限制寄存器会自己变为1.5A

3.输入电流限制0.9A,充电电流限制为0.5A,但实际测量充电时瞬间输入电流高达1.5A左右,且输入电流限制寄存器不会变、

4.输入电流限制0.15A,充电电流限制为0.5A,但实际测量充电时瞬间输入电流高达1.7A左右,且输入电流限制寄存器会自己变为1.5A

5.输入电流限制1.5A,充电电流限制为0.5A,但实际测量充电时瞬间输入电流高达1.7A左右,且输入电流限制寄存器不会变、

以上情况输入电压限制均为4.52V,所以希望可以帮忙解决充电时瞬间大电流的情况,这样会把无线充电拖挂或功率因不够而无法达到9V,1.1A输出;结果会

出现不断的充电和断电。。