This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教DC芯片选型问题



请教,我在选型DC升压芯片,在确定输入输出电压,负载电流,静态电流范围后,还有一堆可用的芯片,请问怎么进一步筛选,

1.有些DC芯片的输入输出电压范围窄,有些输入输出电压可以到60V,对于比如输入5V升压至9V需求来说,输入输出电压范围跟需求更接近的dc芯片,比如输入最高10V输出最高15V,相比更宽输入输出电压范围的DC芯片比如输入最高60V输出最高60V,在精度上或者其他方面有没有区别?

2.请问一般还要什么可筛选的性能,价格因素不需要考虑。

谢谢