This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDO EN悬空问题( TPS70633)



大家好:

我再用TI的LDO TPS70633遇到一个问题,跟大家请教一下:

1、手册中写EN可以悬空,考虑成本,没焊。
2、成板后功能测试,输出正常,3.3V,然后就开始跑机,过了一周多,就发现有4块的输出从3.3V变成了0.5V。
3、怀疑虚焊,用烙铁给其中3块的LDO过了一遍锡,都恢复了3.3V,到现在工作了4个小时,一直没问题。
4,、剩余1块,仔细排查,发现是EN引脚的问题:拉高或者手拿镊子点住EN引脚,输出都能恢复到3.3V;但去掉拉高或移开镊子后,输出又变为0.5V。

请问,为什么,烙铁焊一遍,可以稳定输出3.3V;而拉高或用镊子点一下,3.3V不能一直维持下去。