麻烦推荐一款锂电池充电IC,采用直流电源充电,DC5~24V直流电源均可,单节电池充电,充电截止电压5V以下可调,实际充电电压可调范围2~3V,芯片电压可调范围高点低点也没关系,充电最大电流5A以上,最好10A左右,有对外通讯接口,能监控充电电流、电压值,最终我是50多节电池串联使用,充电时要求单节电池充电,电压电流可调节(用硬件电阻设置),如果没有通讯接口,如何监控充电电流电压值,正在做电路设计,急用,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.