This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS78230



TPS78230,我看手册里说最低压差是0.13V,我想用TPS78230, 当输入是3.13V的时候,输出都能到3V;看手册里电气特性里备注里有:V DO is not measured for devices with V OUT(nom) ≤ 2.3 V because minimum V IN = 2.2 V.;就是说当我输入电压掉到2.8V,那么输出还是2.8-0.13能有2.5几V是这样子嘛;还是说低于输入3V就不能用了