This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23754 PD供电12V

Other Parts Discussed in Thread: TPS23754, TPS23754EVM-383

最近使用TPS23754做了个25W的POE  PD端电路,电路原理图如附件所示。原理图参照TPS23754EVM-383进行设计,由于空间限制,对元EVM中电容进行了重新设计,调试过程中遇到一些问题:

1、想要测量GATE GAT2的PWM波形,将示波器GND连接GND_ISO,此时发现控制器没有任何波形输出,去除示波器使用万用表,能够测量到PWM的电压幅值的变化;

2、电路完全闭合后,上电,后端输出11.7V电压,3~5s后没有输出,经查变压器高压端Q2已击穿,D和S短路,发热严重。

原本想确认PWM波形后再闭合Q2管的驱动10R电阻,但是介于无法使用示波器进行测量,有点头疼。

TPS23754的控制电路采用的是正激式电源电路,按理说Q2的MOS管不应该损坏才对,但是事实就是这个片子发热发烫,然后损坏。

当前个人基本没啥头绪了,只能请各位大侠支招了

TPS23754_POE_25W.pdf