您好!目前客户有退一个异常电池,用EV2300盒子查看电池显示20.4V,但是电量只有4%。
电池没有接负载,电流显示会偶尔有5mA 3mA。
直接用老化设备正常老化,电池从4% 5% 6% 7%后充满更新为100%,再放电,充电。百分比都正常。
这种现象有哪些可能会发生吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
拿到电池老化,直接可以到100%,容量写的4400,但是学习出来只有4300左右。到98%左右会直接跳100%。
但是容量不更新。我reset后,也是一样不更新。0815.gg.zip
CEDV的参数您可以用GPCCEDV调整一下在跑学习试试
www.ti.com/.../GPCCEDV &tisearch=Search-EN-everything&usecase=part-number