This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
按照推荐设计,但是上电后5V一加负载,电感就会啸叫。测试波形电源电压有抖动
空载时12V输入40毫安有啸叫。负载增大到5V 500mA~2A都无啸叫问题。R29并联100pF啸叫声音降低但是还有,并联680pF电容啸叫消失
空载时,5V输出纹波
你的电感值用的有点小,可以用大一点的试试,推荐4.7uH
您好,并联680pF已经没有噪音了。同样的原理图在有的板子上就不需要并联电容就没有噪声