1、目前需要一个7.5V转7V,输出电流4A,请问LM1084合适吗?
2、手册上我看LM1084的dropout电压最小要达到1.5V,就算我把输入7.5V能够调到8.5V满足dropout电压的要求,1.5V*4A=6W的热耗也是很麻烦,请问有么好的方案吗?怎么散热,或者有没有其他片子?
3、LM1084的封装底部也是接输出电压吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
20mV的纹波不需要LDO, 很多的DC/DC都可以做到,实在不行(没有做好的情况下)再DC/DC后再增加以及LC都是可以的。
TPS5450可以做到20mV纹波,尽管datasheet上案例是30mV,如上实在没做好,增加LC进一步降低是可以的。