This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

锂电池(4节)恒流恒压方案(恒流2A,恒压16.8V)

Other Parts Discussed in Thread: UC2842, LMR16030

想找一个4节锂电池恒流充电方案,输入电压范围(DC:25V~55V),输出16.8V2A。

现在想到的是2个方案:UC2842,做buck降压,但是MOS驱动要加驱动芯片(浮驱),成本有点高。

                            然后:看LMR16030,输入电压范围合适,输出电流3A,不知道可以做到16.8V2A=34W这么大的功率么? 因为是内置MOS,频率低了(准备120KHz),峰值电流大,可能烧管子;或者34W,内置MOS损耗大,看的datasheet,例子是输出5V3A,才15W。 还有这款芯片 做恒流,双环反馈(电流环,电压环)会有叫嚣吗,不确定。