This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76940問題諮詢



Hi,

目前我有一電池包項目應用15節電池,目前有以下幾個問題想確認

问题如下:

1,如下图所示,

问题描述,如果红色区域没有连接电芯,红色区域之外连接了电池,以下问题需要确认

1.1 是否影响整机的待机电流?

1.2关机(SHIP Mode)命令发出后,是否会完全关闭REGOUT的输出?

2,现在出现了,发送关机(SHIP Mode)命令发出后,REGOUT的输出电压为1.5V的情况(正常情况为0V),什么情况下会出现?

電池接線圖

謝謝