This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25713的充电问题

Other Parts Discussed in Thread: BQ25713

我们在调试BQ25713的充电的时候遇见如下问题,帮忙解答下,谢谢

1. 当配置充电电流1024的时候,但是实际测试只有800左右。设置成512mA, 实际只有390mA. 测量充电的RSR电阻的电压,  设置充电电流512的时候。 是4mV, 设置1024mA的时候是8.1mV.   设置电流和实际电流不匹配

2. BQ25713上如何判断charge full。 默认截至电流是多少?

3. 是否有recharge功能, recharge电压是多少?

谢谢