Other Parts Discussed in Thread: BQ24172
请问:如何快速的关断MOS管,以免输入电压关掉时,输出电压在MOS管没有彻底关断的情况下又回流到输入端?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: BQ24172
请问:如何快速的关断MOS管,以免输入电压关掉时,输出电压在MOS管没有彻底关断的情况下又回流到输入端?
这个不是BQ24172的,是一个DC_5V和USB_5V的切换电路,当USB_5V这一路去掉时,结果还存在4.6V的电压,因此怀疑是通过MOS管倒灌过来的。
另外,再请教个BQ24172的问题,在手册的figure 3 中,usb输入口接了一个二极管,这样不会因为二极管的压降而影响后级的电压吗?
当USB-5V去掉时,DC-5V通过你的切换MOSFET的体二极管倒灌到USB-5V这一端,那么USB-5V输入端就会有5V-Vdiode的电压,即你提到的4.6V电压。 电源常用的防止倒灌的方法是两个mosfet串联,请你参考BQ24712的电路图中图1或2的Q1和Q2,通过这样的连接防止了倒灌电流的出现。你可以在其中一路加入这样的设计。电流较小时,可以考虑简单的二极管串接。
关于你提到的BQ24172问题,你是指图4的二极管吗?这个二极管就是用于防止倒灌的,也确实会在二极管上消耗正向导通压降的电压和额外的功率,所以这个电路图是用于USb做输入源的时候,即电流比较小的场合,这样消耗的功率才比较小。正如你所考虑到的它使得实际的给到BQ24172的输入电压降低了一个二极管压降,但是我们这个BQ24172能够实现的占空比是非常高,这意味这,即使输入电压降低一些以后,在输出端仍然可以稳定在需要的CV电压。(对于buck电路,CCM模式下的输入输出电压的关系可以粗略用Vout=Vin*Duty cycle来表示,所以Vin降低一些以后,duty cycle会加大一些,这样还是能得到需要的vout.即二极管的电压损失不会影响后级电压)