TI专家:
我准备使用BQ40Z80开发一款产品,但是遇到如下问题:
1.battery management studio 版本是V1.3.86,刚开始找不到bq40z80这个芯片
2.我从TI官网下bqz文件,4800_0_02-bq40z80.bqz,bqstudio里面可以找打 bq40z80,但是出现如下界面,请问是什么原因:
载bq40z80的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这个问题解决了,谢谢。Star Xu 说:可以用,上面的对话框您点ok也是能打开BQstudio的 ,只是固件版本 不同。
还有一个问题,我要怎么配置电池的串数等参数呢,好像是有一个bq40z80 TRM sluubt5a.pdf这个文档,但是链接进去打不开,没有文件啊,能否提供一个下载链接,谢谢。
你好,我在测试demo板的时候遇到如下问题,TS3和TS4 温度显示不正常,下面bit也是报错的。现在的状态是不充电。
我测试过TS3和TS4,热敏电阻阻值正常,和bq40z80的相应Pin也是通的。
jumper也是按照相应的要求配置改过;芯片已经unsealed,相应的电池串数和DA值也改过。
请帮忙分析一下原因,谢谢。
我是5S的电池,设置如下:
When you enable TS4, do you have a thermistor connected to TS4? Is it possible you are encountering an open thermistor permanent fail (see Section 4.22 of the TRM)? The device might be opening the FET in response to this fault condition. The other thing to consider is that TS4 and TS3 are multi-function pins so they must be configured for temperature sensing before you can enable to the temperature sensor.