This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC2843A做反激开关电源16V输入时,满载输出时输出电压会拉低2V?

Other Parts Discussed in Thread: UC2843A

UC2843A做反激电源时如果MOS耐压足够余量,是否可以把占空比调制到大于50%至90%,100%? 输出满载3A时拉低到6VDC,输入电压升值20VDC时可以稳住输出8V3A,

:输入VminDC16v-Vmax60VDC,输出8VDC3A隔离驱动电源,,是否因为占空比低压输入时太小,变压器匝比N=1.75,,初级LP=230UH,选用400V12AMOS场效应管,足够大的余量时是否可以设置超50%的占空比,首先前提增加了斜率补偿电路的,求教多谢!

  • 首先,用400V管子并非稳妥之举,尤其以电压电流论英雄却在高频应用中忽略了MOSFET损耗本质,这就如同泰森很壮;力气很大很牛气,可你把他派来调板子。。。呵呵→_→当心他追你哈哈(ಡωಡ)hiahiahia

    MOSFET额定电压电流只是特定条件下的耐受极限,关键参数绝非仅这两个,人家制造商可是弄了厚厚本数据表滴呕。

    其次,占空比最好不要超过60%。这与管子耐压没啥(^・ェ・^)关系,斜率补偿也救不了。。。关键是有二次元(次谐波)振荡分险。

    再次,低压出力不够,有多种可能。比如电流取样电阻值偏大;变压器饱和;PCB设计不合理;ESL或ESR分部不合理或者原理设计有缺陷;测量方法有误。。。

    尤其用万用表测个电压就BB,那就更不靠谱了。除非特质,毕竟市面电压、万用表能感知的最高频率仅20kHz。

  • 说了那么多,只有一个中心。原理、PCB、波形都上哪去啦?快去上传!
  • Hi
    感觉主要还是变压器设计。不建议duty过小,但是宽范围供电,势必duty会超过50%,谐波补偿还是建议的。
  • Hi
    感觉主要还是变压器设计。不建议duty过小,但是宽范围供电,势必duty会超过50%,谐波补偿还是建议的。
  • 可一旦超过65%,就有很大次谐波振荡分险。所以;宽范围下,利用窄占空比是必须的。
  • 会不会是初级电流被限制了,测量一下UC2843A各点的波形来看看。