This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MAX Error 3% 代表什麼? 關於BQ78350-R2



大家好,

關於BQ78350-R2,參考網上資源得知

MAX Error=100% 未學習

MAX Error=8% 仍在學習中

MAX Error=2% 學習完成

------
電池組發生某一Cell Voltage 突然驟降又回復,有觸及 EDV2 電壓,SOC 更新到7 %

而MAX Error變為3%  請問代表什麼狀況?