This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI-TPS61062的可控白光LED照明灯

Other Parts Discussed in Thread: TPS61062

TI-TPS61062的可控白光LED照明灯

1.作品摘要介绍:

我们设计并制作一个高效可控白光LED照明灯及其检测装置,采用5V单电源供电,用TI的TPS61062芯片驱动4~5只白光LED进行照明。

2.总体方案设计:

    本系统采用单片机C51为系统控制的核心,此系统主要包括TPS驱动模块(即PWM的输出),ADC0809的采样模块,LED的功率检测和现实模块,简单的光度检测仪模块等。

2.1总体设计方案的介绍:

  本作品的设计思想是通过TI的TPS61062芯片驱动4~5只白光LED进行照明,并能对输出到LED上的功率进行测量、显示和对输出到LED上的电流进行预置、控制。用光敏器件制作一个照度检测仪,它可以将检测到的照度显示。

2.2系统控制方案:

     采用C51实现系统控制。C51板子上有自己的ADC0804。不过,ADC0804只有一个8位的ADC采样端口,也就是说它只能采集一处电压。如果用来采集光敏电阻出的电压,那么它就不能用来采集LED白关灯的电压,从而不能做功率检测和实现。同理,如果ADC0804用来采集LED白光灯的电压,那么系统又不能根据外界的光照的改变而改变LED白关灯的亮暗程度。所以,决定用ADC0809来做采集。ADC0809是一个有8口8位采样的芯片,对于用来采集两处的电压,绰绰有余了。ADC0809对数据的测量精度高;采样的速度快。

2.3ADC0809芯片说明

ADC0809各引脚功能如下:

D7-D0:8位数字量输出引脚。

IN0-IN7:8位模拟量输入引脚。

VCC:+5V工作电压。

GND:地。

REF(+):参考电压正端。

REF(-):参考电压负端。

START:A/D转换启动信号输入端。

ALE:地址锁存允许信号输入端。

(以上两种信号用于启动A/D转换)

EOC:转换结束信号输出引脚,开始转换时为低电平,当转换结束时为高电平。

OE:输出允许控制端,用以打开三态数据输出锁存器。

A、B、C:地址输入线。

可控白光LED照明灯报告.doc