1. 我正在做产品设计,在电路中我想用一块lm117,我在datesheet里面看到lm117是有sot-223封装的,我需要量比较少,不知道现在texas还有在生产销售lm117 sot-223封装的产品吗?
2. 如果没有是否可以考虑用lm317 sot-223的替代,lm117好lm317主要的区别在什么地方?
期待您的回复。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
LM117与LM317的主要差别在于温度级别导致的应用范围不同,LM117结温范围是-55~150℃,而LM317则是0~125℃,另外就是要注意不同的封装下最大的输出电流时不同的。
LM117是没有SOT-223封装的。如果你要考虑用LM317替代,首先要确认温度是否合适,或许你可以考虑用LM317A,它是有SOT-223封装的,结温范围是-40~ 125 ℃.