This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65261问题请教



问题 1.手册 19页 “Power for the high-side and low-side MOSFET drivers and most other internal circuitry is derived from the V7V  pin. The internal built-in low dropout linear regulator (LDO) supplies 6.3V (typical) from VIN to V7V. A 1μF  ceramic capacitor should be connected from V7V pin to power ground.”

如果系统Vin输入为5V,是否这个V7V_LDO就不工作了?

问题2:如果系统输入是5V,MODE pin接地,出于 简单考虑,能否将EN1~3都悬空,这样3个buck的输出能否正常工作?

  如果这种情况下3个buck能正常 工作,这是3者的上电顺序是否是同时上电?