This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

芯片BQ24650做电源管理,充电没有恒流工作?

Other Parts Discussed in Thread: BQ24650

用BQ24650对单个锂电池充电管理,设定输出电压=2.6V,通过RW1电位器调节输出电压,空载时用万用表测量输出得到2.6V电压;设定充电电流2A(选用取样电阻20mΩ阻值)。我的问题是,当接入电池后,电压在2V时充电电流=1.8A,电压=2.4V时充电电流=1A,我的理解应该是电压2V是恒流2A充电,电压上升电流保持不变(这才是恒流充电),当电压到2.6V时,电流再缓慢下降,直到充电截(恒压模式),为什么我的电路不是恒流工作?原理图见下图:

请帮助查找原因,急切等待您的回复,谢谢!

  • 您参考bq246xx Calculation Tool V1.5看一下参数配置是否合理。

    http://www.ti.com/product/BQ24650/toolssoftware

  • 非常感谢你的回复,参考这个工具,将R7阻值调整到79.5K,目的是设定MPPT电压=23.8V(电路中BQ24650输入电压是DC/DC稳压给定24V),其他参数都是合理的,现在现象是电池2.4V时电流0.55A,电池2.475V时电流0.29A脉冲充电,亮灭间隔约1s。还是没到恒流2A?
  • 麻烦TI技术支持给予帮助,确认电路故障原因,号码,谢谢!
  • 我怀疑充电线太长了。
    1. 实验测试:
    我做仿真调试,使用电子负载模拟锂电池,设置电子负载的恒压模式= 2.6 v,调整RW1电位计来提高输出电压设置,在这个时候,充电电流是观察到慢慢上升,2.2A是最高的(这个测试是验证BQ24650能否输出最大电流)。
    2. 问题总结:
    设置输出电压电路= 2.6 V (2.1 * (1 + RW1/R1)),充电电流= 2A (Rsr1 =20 mΩ),我的BQ24650电路和电池之间充电线长约1米,用万用表测量电池电压=2.4 V,用万能表测量SRP和SRN电压=2.56 V .我的判断是BQ24650已经转恒压模式在减小电流了。
    3。我的问题:
    如果充电线很长,如何设置输出电压和解决电压降问题?
    非常需要帮助,谢谢!