电路中使用了一个P沟道MOS管,在S极加了5.3V的电压,在G极产生了5.02V的电压,这样MOS管应该处于关闭状态吧?但是我量了下D极,发现还有1V左右的电压,这个电压是不是漏过来的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
电路中使用了一个P沟道MOS管,在S极加了5.3V的电压,在G极产生了5.02V的电压,这样MOS管应该处于关闭状态吧?但是我量了下D极,发现还有1V左右的电压,这个电压是不是漏过来的?
请问你用的什么型号的MOSFET?
处于亚阈值导通的导通状态的MOSFET漏源之间(DS)等效成一个可变电阻,如果接一定负载,就是两个串联电阻分压,所以你测到的1V就是负载分得的电压。
Hi
FDC697P 的 VGS(th)电压规格是-0.4 ~ -0.8 ~ -1.5V,Q24 在VGS-0.3V时仍然存在漏电流,Q23的体二极管因为漏电流导通而形成的电压(即体二极管电压)。
Johnsin, 如果是Q23的体二极管导通了,节点7的电压比Q23的1,2,3,5,6的电压高才是,但是如楼主所言,节点7的电压只有1V,所以我认为是在测试的过程中,由于万用表成为了一个负载,Q23处于弱导通状态,漏电流在万用表上形成的电压。
我觉得可以认为你这两个背靠背的MOS管已经达到了彻底关断的状态。
@chenchen
你只是在Q24的S加了5.3V电压,G极没加电压?在Q23的S极就产生了电压?另外,因为是浮地的,可以把电路图贴完整一些看,描述一下你的输入和输出。
读一下数据手册就知道FDC697的栅和体之间是存在漏电的,不是绝缘。所以从Q24的S极到Q23的S极相连的,通过电阻。
另外,Q23体二极管会有反向漏电流,只是比较小,而且方向肯定是从电势高到电势低。
当表笔搭上后端点7会被拉低。
Hi 遇到这种问题吧,建议看看我的帖子,希望对你有帮助
你看看这个贴子:
【原创】MOSFET的驱动技术详解
http://www.elecinfo.com/bbs/582407.html
【原创】使用大功率MOSFET时的设计依据