使用DC-DC升压芯片MAX1606,将5V升压到27V左右。发现MAX1606外围电路上的电感对芯片性能影响很大。在MAX1606后加了一个5mA恒流管期望实现一个恒压恒流源作为传感器驱动使用。问题:刚才说的MAX1606那个外围电路上的电感使用10UF时,输出的27V被负载拉低到11V。使用220UF时输出没有被拉低,但是纹波噪声显著升高,而且电流增大了很多。我想请专家帮助我理解一下这个现象,或者推荐一些相关资料给我学习。谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用DC-DC升压芯片MAX1606,将5V升压到27V左右。发现MAX1606外围电路上的电感对芯片性能影响很大。在MAX1606后加了一个5mA恒流管期望实现一个恒压恒流源作为传感器驱动使用。问题:刚才说的MAX1606那个外围电路上的电感使用10UF时,输出的27V被负载拉低到11V。使用220UF时输出没有被拉低,但是纹波噪声显著升高,而且电流增大了很多。我想请专家帮助我理解一下这个现象,或者推荐一些相关资料给我学习。谢谢
首先说明本社区暂时只针对德州仪器的产品提供咨询。
然后试着解答一下问题,但是仅供参考。
根据数据手册,MAX1606的限流采用的是电感电流峰值。在相同开关频率下,较大的电感其纹波电流较小,因此在同样峰值限制下,采用较大的电感能够相同开通时间内存储更多的能量。会有更强的输出能力。数据手册同时提到,改变LIM引脚可以设置不同电流值,您或许可以试一下。
另外对升压变换器,在大变比下采用大电感往往会形成低频右半平面零点,影响稳定性,不建议选用。
最后,如果可能的话,请试用我司的TPS61170,1.2A High Voltage Boost Converter in 2x2mm2 QFN Package。