Other Parts Discussed in Thread: TPS61170
使用DC-DC升压芯片MAX1606,将5V升压到27V左右。发现MAX1606外围电路上的电感对芯片性能影响很大。在MAX1606后加了一个5mA恒流管期望实现一个恒压恒流源作为传感器驱动使用。问题:刚才说的MAX1606那个外围电路上的电感使用10UF时,输出的27V被负载拉低到11V。使用220UF时输出没有被拉低,但是纹波噪声显著升高,而且电流增大了很多。我想请专家帮助我理解一下这个现象,或者推荐一些相关资料给我学习。谢谢