This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5170不能正常带载



设计是5V100A,输入14V。现在到通道能带30A,两通道才带40A。单通道到35A时,发现有占空比被限制了,csa1和csb1两脚的电压达到50mV,启动被限制了,上管才开一个小波。两通道40A时,发现2通道波形正常,1通道的下管占空比被限制得很低。怎样解决两个问题?1,cs脚检测到反向信号,而电感电流波形正常。2,两个通道感染的问题