This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

推荐一款 方便焊接的电源

Expert 2137 points

Other Parts Discussed in Thread: TLV62569A, TLV62569

电源具体要求 输入3.3V-5.5V ,输出两路 (1)一路3.3v 电流500mA (2)另外一路1.2V 电流1A 。 重点是输入3.3V 也能正常工作

  • TLV62569、TLV62569A等都是不错的易焊元件。可以试试。
  • Hi
    在电源管理的降压芯片(集成)下选择,在条件中OUTPUT选择2, 然后再选择你喜欢焊接的封装,再看电流是否合适,很容易找。
    但要注意,如果你要输出3.3V,建议你输入适当高一点,即便100%duty, 输入也需要一定压差。
    对于焊接,看你习惯,很多人喜欢热风枪,也有人喜欢烙铁。