您好,我使用TI的UC3875PWM控制器输出经光耦隔离给如上的电路,可上电发现只要一接上+12的电压,UCC27210芯片就会烧掉或者UCC27424输出与输入的频率不一致,请问这是怎么回事啊,难道我的电路设计的有问题?请您帮我看看,谢谢
图片请见附件
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
在你的测试中,建议你做分段测试, 首先确认光耦隔离的效果,然后确认UCC27324的工作状况,最后确认UCC27210的动作状况。
最好是你手头有数字信号发生器,按照控制芯片的PWM输出,模拟一个占空比给到光耦(否者你就要通过外给信号让芯片动作起来有PWM输出),测试占空比变化,主要是占空比大小和相位,如果没有问题在看UCC27324,UCC27210的动作。
按照你现在的电路,很难看到问题,首先光耦输出的波形是否符合UCC27324 2V高1V以下低电平的逻辑要求,以及占空比没有重叠部分等等。另外你的UCC27210烧掉时,所控制的MOS是否一并烧掉等等。
最后,关于芯片,如果可以的话建议你在TI官方网站上申请,否则你需要到TI授权代理商处购买,如果是电子市场,很容易买到假片或者坏片,按照你的测试正常而言UCC27324不应该坏,因为如你所说他仅仅只是做电平转换,如果没有过压很难烧坏的。
不是说电路有问题说不得,关键你你提问的方式就让我很不想回答你的问题,不见!