This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5116 电感选型问题,电感发热严重是否正常?



按照TI AN-1713文档里设置的参数,文档里是12V@5A输出,我是13.5V@3.5输出,但是参数是按照文档里设置的,想着测试没问题后再改成输出13.5V的。

先说下,MOS和电感选型是直接用的我手头现有的,所以这两个元件参数不合适,MOS的RDSon=8.5mR,Qg在10V时104nC;电感参数见图示。

现在45V输入,12V@1A输出时,电感很快就很烫,频率由250KHz切换成200KHz后,只是热得慢些,大概20秒后也烫了,大概60度。12V@2A输出时温度升上去得就更快了。我看大家电感选型都是选的内阻10mR左右,而且体积超大的。发烫是因为我电感选型不对,还是参数没调好导致的?大家选内阻小体积大的就是因为发热大吗?第一次用这种外置MOS的DCDC控制方案,请大家给点指导。