This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50放电过流恢复问题

现象描述:

电池是个3串锂电池,使用12.6V充满后;做放电过流测试;放电过流保护后;不能充电。这个状态寄不能使用12.6V充电也不能再放电,对客户来说是这个砖头了。

原因大致:

1、放电过流恢复电流设置为10mA,即要充电才能恢复;

2、CHGFET位为0,  充满100%后不关充电MOS管;

3、充满做过流测试后,电芯总电压12.3V左右。 

4、充电器电压12.6<12.3+放电MOS管体二极管压降(0.6V左右)。故无法充电。

其他

电路预充电电路共用充电MOS管。

请教各位大神有没有什么办法解决这个问题,客户就在充满的这个点测试 。放电过流一定要充电激活。