Other Parts Discussed in Thread: UCC21521
我们使用UCC21521ADW做半桥电路的驱动,高边的驱动采用自举供电的方式,当输入电压升高或者负载电流增大时,发现驱动输出会偶然性中断几十us,然后恢复,我们确认此时输入信号的Vcc是正常的。当我们把UCC21521远离功率MOS管,上述现象消失,请问应如何处理?
补充信息:
1)我们采用DT脚设置死区,R=18.2k, C=2.2n, 两路输入是从逻辑电路出来的50%互补的型号,正常情况下在功率管上看到200ns的死区;
2)功率器件是650V的SMD器件,驱动芯片和MOS管分别位于PCB两面,二者靠得很近,当把驱动芯片和周边电路远离MOS管5~6cm后,异常情况消失;
3)两片UCC21521都只有一个通道出问题,其中一个在低边,另一个在高边,但都是VOB,不知是否巧合;