This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ21040的充电电流突降问题

Other Parts Discussed in Thread: BQ21040

BQ21040芯片实测充电曲线如下,(VBUS  5V),可以看到充电电流出现异常:

针对充电曲线中充电电流异常有如下问题:

1,VBUS=5V,VBAT=3.13V, 充电电流615mA,恒流阶段充电电流未达到设计值800mA,为什么?是否芯片无法支持VBAT低电压下最大800mA电流充电?或者芯片在VBUS-VBAT大压差时散热异常?

2,VBUS=5V,VBAT=4V,充电电流开始下降,此时并未进入恒压阶段,为什么充电电流下降?

3.  VBUS=5.3V,VBAT=4V,充电电流恢复到800mA,维持最大电流充电对VBUS输入电压的要求是多少?

电压电流测试数据如下:

VBUS(v)

VBAT(v)

Ibat(mA)-D2002在位

Ibat(mA)-去掉D2002

5

3.13

615

537

5

3.23

671

565

5

3.33

735

600

5

3.43

808

639

5

3.54

808

685

5

3.65

808

741

5

3.74

790

803

5

3.83

732

808

5

3.96

674

807

5

4.03

600

782

5

4.16

539

723

5

4.2

471

434

BQ21040原理图设计如下: