This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76940方案

Other Parts Discussed in Thread: BQ76940, LM2904B, LM2904, BQ76952, BQ76930

关于BQ76940的参考设计,

http://e2e.ti.com/blogs_/b/industrial_strength/archive/2019/11/21/fast-and-furious-designing-longer-lasting-16s-17s-li-ion-battery-packs-for-e-motorcycles

有一些疑问是否可以解答一下,谢谢!

从系统图上看2904只用于做比较器的功能是么?理解有没有问题,若电池接反,则Q1关;若接正确,则Q1打开,R89(237K)和R96(115K)进行分压,供给ADC采样;从原理图上看这样的分压后电压很高,一般的ADC输入承受不了这么高电压,精度是按这个电路测的么?

2904的供电,从电气性能上看,2904最大工作电源26V,17串电压显然大于48V;运放输入脚对地电平也不够;如果接到比如13或14脚,功耗应该会不一致;

如果Cell13和CEll17rc反接,运放应该容易烧,这也算是一种操作上的风险,需要提醒现场操作人员;

电路的温漂性能如何;

实验时D29和D31稳压管是否有接,对精度应该有影响;