Other Parts Discussed in Thread: UCC39002, LM73605, LM324, LM61495, LM61495-Q1
你好!我想用UCC39002来并联两个由LM73605的DC/DC电源电路,但看了UCC39002的文档后,有一个疑问:
UCC39002的文档有这样一段话:
The SENSE(+) terminal of the module is connected to the ADJ pin of the load share controller. By placing a
resistor between the ADJ pin and the load, an artificial SENSE(+) voltage is created from the voltage drop across
RADJ due to the current sunk by the internal NPN transistor.
我的问题是:
1)我不明白的是LM73605电路中哪个节点可以充当一般电源模块的SENSE(+) 端子?FB引脚?是不是UCC39002不适合用于LM73605的并联均流?只适用于有SENSE 端子的电源模块?
2)LM73605是否可以直接并联使用?如不能有什么适合LM73605并联均流的方案可以推荐?
谢谢!期待TI专家的回复~