This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610的安全定时器问题

Other Parts Discussed in Thread: BQ24610

项目需要充电时间大于10小时,而bq24610最大充电时间为10小时。手册提到:

The TTC pin may be taken LOW to disable termination and to disable the safety timer. If TTC is pulled to VREF,
the bq24610/7 will continue to allow termination but disable the safety timer. TTC taken low will reset the safety
timer. When ACOV, VCCLOWV and SLEEP mode resume normal, the safety timer will be reset.
TTC拉高和拉低这两种情况有什么区别不懂,谁能讲解一下。
  • 将TTC pin 拉低就是取消安全定时器功能和充电截止功能。
    将TTC接到VREF允许充电截止功能但是取消安全定时器功能。
    您的设计>10h,建议使用第二种,将TTC接到VREF,取消安全定时器功能